AXIS#.SAFEPARAM.SSR_#.TIMEFORVELINLIMITS

Description

Indicates the time for the velocity in limits for the Safe Speed Range (SSR) safety function. After this time, the monitoring can be activated if the velocity is already in the limits.

 

This value is t_L_SSR in the following diagram:

Context

For complete SSR information refer to SSR (Safe Speed Range).

Related safety parameters:

Versions

Action

Version

Notes

Implemented

2-04-00-000

Implemented in SMM revision v0.56

General Information

Type

Read/Write

Units

Milliseconds

Range

[1, 60000]

Default Value

1

Data Type

Integer

Stored in Non-Volatile Memory

No

Fieldbus Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

AXIS1.SAFEPARAM.SSR_1.TIMEFORVELINLIMITS

3161h

08h

Unsigned16

-

-

Read/Write

No

AXIS1.SAFEPARAM.SSR_2.TIMEFORVELINLIMITS

3162h

08h

Unsigned16

-

-

Read/Write

No

AXIS1.SAFEPARAM.SSR_3.TIMEFORVELINLIMITS

3163h

08h

Unsigned16

-

-

Read/Write

No

AXIS2.SAFEPARAM.SSR_1.TIMEFORVELINLIMITS

3261h

08h

Unsigned16

-

-

Read/Write

No

AXIS2.SAFEPARAM.SSR_2.TIMEFORVELINLIMITS

3262h

08h

Unsigned16

-

-

Read/Write

No

AXIS2.SAFEPARAM.SSR_3.TIMEFORVELINLIMITS

3263h

08h

Unsigned16

-

-

Read/Write

No